World’s First Hidden Door Hinge Line Up!
Posted On Jun 23rd 2025
July 29, 2026: Due to a power outage caused by severe weather conditions at our Illinois facility, we will be unable to ship from this location until power is restored. Please notify us of any expedited orders that must ship today so we can ship them from our California warehouse. We sincerely apologize for this inconvenience.
Posted On Jun 23rd 2025
Posted On Jun 23rd 2025
Media Contact:
Curtis Nakamura
Tel: 562.544.8909
Email: c.nakamura@sugatsune.com
Sugatsune America Introduces HES 1, 2, 3 Campaign
August 6, 2024 – Atlanta, GA. Over its 94-year history, Sugatsune has become known worldwide in the industry as an innovative hardware manufacturer. In 1992, Sugatsune introduced the world’s first adjustable hidden hinge, the HES3030 AK/SC making it easy for builders and installers to ensure proper alignment of doors and their reveals. Followed up by the HES3D series of 3-way adjustable hinges which features an industry first 7-axis arm design and lift off feature with a temporary hold function. This allows for tighter reveals and easy installation as a full-size door could now be hung by a single person.
“Sugatsune’s DNA is synonymous with innovation not as a common buzzword but as a core pillar in the development of new ideas and trends,” says Curtis Nakamura, Sr. Vice President. “As hidden doors have become popular, Sugatsune continues to show its innovation with a comprehensive line-up of hidden door hinges ranging from traditional mortised hinges and surface mount frame hinges to now a complete system that includes an invisible hinge that is incorporated into the door frame. This new system creates one of the thinnest reveals, winning an iF Design award in addition to the Kid’s Design award for safety.”
Earlier this year, Sugatsune added to its line-up, a 304-grade stainless steel hidden door hinge which can stand up to environmental elements. As with the HES3D-E190 and HES3D-W190, this all-new HGS3D-S160SH is UL rated for 3-hours making it a great application for commercial projects.
About Sugatsune America, Inc. With a heritage dating back to 1930 and established in 1982, Sugatsune America Inc. is AS9120 B; ISO 9001:2015 certified and has a rich tradition of manufacturing and distributing Japanese quality hardware. Sugatsune America stocks over 6,000 unique parts locally in the U.S. to provide the highest level of service. LAMP® is a registered trademark of Sugatsune Kogyo, Inc. For more information, visit www.sugatsune.com. Connect with Sugatsune America via Facebook (facebook.com/sugatsune), Instagram (instagram.com/sugatsuneamerica) and Twitter (twitter.com/sugatsune).
North American Headquarters:
18101 Savarona Way
Carson, CA 90746
Tel: 310.329.6373, 800.562.5267 (USA only)
Email: sales@sugatsune.com
CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)