Detent Motion vs. Torque Positioning: How to Specify the Right Hinge Motion
Posted On Sep 1st 2026
Posted On Sep 1st 2026
Posted On Sep 1st 2026
Mechanical hardware does more than connect two components. In industrial equipment, medical devices, control panels, kiosks, and display systems, hinge behavior can determine how an operator interacts with an assembly. A panel that stops at predefined positions behaves differently from one that holds continuously at any angle. At the same time, a monitor that needs rotational adjustment requires a different mechanism from a lid moving on a single axis.
That distinction is where detent motion, torque positioning, and swivel movement become important. Sugatsune’s Motion Design Tec® approach separates hinge behavior by function. Sugatsune describes click motion as a detent-based mechanism that moves between set positions and holds a panel at those defined angles. Torque hinges instead use friction to resist movement and hold a lid, panel, or display at a selected position without a separate stay or stopper. In the Motion Design Tec® world, this is called free-stop motion.
A detent hinge creates mechanical stopping points through its range of travel. Rather than allowing the attached component to remain at any arbitrary angle, the mechanism engages at predetermined positions. Sugatsune notes that the clicking action gives users a clear indication that the panel has reached and is being held at a set position.
This behavior is useful when an application benefits from repeatable positions rather than infinitely variable adjustment. A machine cover may need to stop at the same service angle each time, or a display may need several defined viewing positions. The detent provides tactile feedback without requiring a separate latch at each setting.
A positioning torque hinge uses friction to control movement by resisting the rotational force created by the moving lid, door, panel, or display. When the hinge provides sufficient resistance, the component can remain where the user leaves it.
This free-stop behavior is useful when an operator needs many usable positions instead of several predefined stops. Applications can include machine access panels, display supports, lids, lighting equipment, medical devices, and other assemblies where flexible positioning matters.
Select a positioning torque hinge based on the type of movement required and the amount of torque moment created by the moving component. A simple way to calculate this is to take the measurement of the lid or panel from the hinge to the edge, multiply it by its weight, and divide the result by 2. It's recommended to note the tolerances when specifying friction or position hinges to ensure the torque moment stays within the hinge’s torque tolerance range.
Too little resistive torque can allow a panel to drift or fall. Excessive torque can make movement difficult or jerky. Engineers must account for mass, center of gravity, mounting orientation, geometry, and the number of hinges in the assembly.
A swivel torque hinge is intended for applications where a component must rotate around an axis while maintaining controlled positioning.
Sugatsune’s HG-S series includes models with 360-degree rotation and free-stop functionality for industrial control panels and monitors. The HG-S50-75 also incorporates a center cable opening, allowing wiring to pass through the hinge area while the supported component rotates.
Selecting a swivel torque hinge requires more than confirming its rotation angle. Engineers should review rated torque, load orientation, mounting geometry, cable-routing requirements, environmental conditions, and product-specific torque tolerance. For the HG-S50-75, Sugatsune states that initial torque may vary by ±20%, showing why tolerance needs to be incorporated into the design rather than treated as a nominal-only value.
Engineers comparing rotational hardware can review Sugatsune’s friction and torque hinges and broader hinge selection.
A 360-degree swivel hinge provides full rotational adjustment around its swivel axis. The engineering question is whether the hinge merely rotates or also generates torque that holds the attached component at a selected orientation.
Sugatsune’s HG-T30S15 dual-axis torque hinge illustrates the second approach. It can tilt and swivel while using friction to retain its position, with a specified 360-degree swivel range. Sugatsune lists ordering kiosks, information screens, medical diagnostic monitors, manufacturing control panels, flat-panel displays, and interactive touch screens among its applications.
Evaluate a 360-degree swivel hinge across its full motion envelope. Engineers need to check cable twisting, interference with enclosures or nearby controls, minimum cable bend radius, operator reach, and the consequences of unrestricted rotation. Where wiring passes through or near the rotational axis, consider cable management when selecting the hinge.
Neither mechanism is universally better because each solves a different control problem.
Use a detent mechanism when operators should feel and recognize specific indexed positions. It is appropriate where repeatability matters and only several working angles are required.
Use continuous torque positioning when a component must remain at many possible positions throughout its travel. A friction hinge can provide this behavior without a separate mechanical stay, provided its resistive torque matches the application moment. Note, however, position hinges create a spring-back phenomenon where the door or lid doesn’t stay completely shut because of the opposing force. For situations that require full closure, pair it with a mechanical or magnetic catch.
Use rotational torque hardware when a monitor or control panel must be redirected around a swivel axis while remaining stable at the selected angle.
For additional design guidance, review Sugatsune’s How to Specify Friction Hinges and The ABC’s of Torque Hinges.
Start hinge selection with a precise definition of the desired movement. A mechanism designed for indexed positions should not automatically be substituted for one designed for continuous free-stop control. Likewise, conventional friction hardware cannot necessarily replace rotational hardware when an operator interface needs a full swivel range.
Sugatsune’s Motion Design Tech® framework organizes hardware around behaviors including free-stop, assist, soft-close, and detent-based movement, allowing engineering teams to identify the required motion before selecting a specific component.
When an application combines multiple motion functions, evaluate each axis independently before selecting the final hardware.
For application-specific assistance, contact Sugatsune America to discuss load, mounting, positioning, and motion requirements with a technical representative.
Click motion relies on detents that hold a component at defined angular positions and give the user tactile feedback as the hinge moves between settings. Torque positioning uses friction-based resistance and can hold a component at many points throughout its permitted range. The appropriate mechanism depends on whether the design requires repeatable indexed positions or variable adjustment.
Calculate the moment generated by the lid, door, panel, or display based on its weight and center of gravity relative to the hinge axis. Compare that result with the hinge’s published torque and tolerance. Sugatsune recommends keeping the application moment below the low-end torque tolerance to maintain reliable free-stop control.
A 360-degree swivel hinge is useful when a display, control panel, or interface must face multiple operators or work positions. Engineers should verify the required holding torque, available clearance, cable routing, and whether the application needs free-stop resistance or defined indexing throughout the rotational range.
CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)