Everything You Want to Know About Pocket Doors, Hardware & Sliding Door Kits
Posted On Dec 19th 2025
July 31, 2026: We are please to announce that our Addison facility is back up and running. Thank you for your patience and understanding. Please contact us if you have any questions or concerns about your orders.
Posted On Dec 19th 2025
Posted On Dec 19th 2025
Pocket doors, hardware, and sliding door kits open up new possibilities. Maximize your space in a whole new way. Professional designers and detailers, as well as DIY-heads, must understand how the optimal hardware is critical for flawless function. This comprehensive guide removes the mystery from pocket doors, from hardware colors to sliding door options and more.
Sugatsune America is one of the top brands of precision-engineered door hardware. We'll discuss durability and everything you need to know for a sleek, space-conscious finish on your next project.
Why aren’t pocket doors more popular?
Pocket doors are currently resurging in popularity, primarily for the space they save. This is especially true of modern and minimalist design. Some reasons why they aren't as universal as hinged door types include:
Some types of pocket doors have been prone to warping. Others struggled to stay on the track. There's a lingering perception that pocket doors are not dependable.
What hardware do I need for a pocket door?
No matter the type of pocket door, you'll need these components: a set of tracks along which the door slides, and a handle or pull to slide the door open or closed.
The quality of the hardware is essential for performance and durability. Choose Sugatsune America, one of the top brands of door hardware, for superior results.
What is the disadvantage of a pocket door?
Another potential deficiency is the perception of sturdiness (or lack thereof). In standard 2x4-framed walls, the section of the wall housing the door lacks the solid vertical studs found elsewhere. This can make that portion of the wall feel less sturdy or "wobbly."
What type of door is best for a pocket door?
Customarily, the most recommended door type for a pocket door installation is a solid-core option (especially when paired with the best door hardware brands). Solid-core doors are better equipped for hardware, providing superior sliding door options. The added weight helps the door slide better.
Where can you not put a pocket door?
Here's where we wouldn't advise the installation of a pocket door:
Pocket doors also lack a tight seal. These sliding doors wouldn't be the best option for rooms where moisture control or privacy are vital to building use.
What color door increases home value?
It's important to note that door color (and hardware color) will also depend on other factors. Primary ones include the interior design of a room or a building's architectural style. Intended use is also a factor. Consider these hues:
Whites and off-whites offer a neutral and clinical look. This is preferred for specific commercial and industrial spaces. Be careful with bright and bold shades. Also, account for hardware color (handles and pulls) when selecting pocket doors.
Do pocket doors require thicker walls?
Most pocket door types do not require thicker walls. Standard interior walls with 2x4 framing will suffice for most pocket door installations.
You may need a thicker wall when:
What pocket door hardware is timeless?
The timelessness of door hardware is less about a specific style than about the enduring qualities of its design. It's more about selecting clean and classic hardware colors and finishes that transcend trends:
Sugatsune America is one of the top door hardware brands, delivering high-performance with classic style.
What is the most timeless hardware color?
The most timeless color/finish for pocket door hardware can be broken down into two main enduring choices.
Satin or brushed nickel is the enduring classic. Its soft, muted finish is versatile, complementing cool and warm palettes. It provides a seamless contribution to any type of interior. Satin/brushed nickel is also easy to maintain.
Oil-rubbed bronze adds warmth and richness, particularly to traditional and farmhouse interiors. Its old-world feel is always in style. Develops a patina from years of touching for a lived-in feel.
Do pocket doors increase home value?
Pocket doors may not dramatically increase your home's appraised value. They boost your home's appeal and functionality to potential shoppers. That can mean more competitive offers and a faster sale.
Their value is less about a dollar-for-dollar return and more about improving the quality of life and usable space in the home.
Here's why pocket doors may be a net positive for your residence:
Well-installed doors and thoughtfully selected hardware colors convey a high level of attention to detail.
Which is better, a pocket door or a barn door?
Your preference between a pocket door and a barn door will be dictated by your priorities for space and privacy. There's no single "better" option between the two, as they usually accomplish different goals.
Barn doors are often easier to install. This may be more cost-effective. Pocket door installations require opening a wall to hide the door frame and track. This can be much more difficult for an existing home.
Pocket doors are more minimalistic. Barn door options contribute a rustic appeal that can sometimes clash with contemporary or sleek interiors.
How much does it cost to install a pocket door?
The cost to install a pocket door hinges on whether you are doing new construction or retrofitting an existing wall. The national average cost for a pocket door installation ranges from $800 to $2,500.
Expect to fork over more for complex remodels and high-end materials. Using less common hardware colors or finishes can also increase overall costs.
The required labor for pocket door installation is the most crucial factor for your bottom line:
Existing remodeling: This process requires significant work beyond door hanging. There's demolition and structural framing to accommodate the pocket. Relocation of plumbing and wiring will increase costs. If the wall in question is load-bearing, additional fees may be incurred for structural changes or for consulting a licensed architect or engineer.
New construction: There's less work as the walls should already be open to accommodate any type of pocket door. The contractor can easily install the frame and hidden rails.
The decision to use a pocket door depends on your need for a sleek, space-prioritizing design. The bonus of a door that completely disappears into the wall is premium, especially when small spaces and unobstructed walls are critical. Keep in mind that longevity and smooth operation call for quality pocket doors, hardware, and sliding door kits.
Ready to move forward with a custom door solution for your next primary residential or commercial job? Contact a sales expert at Sugatsune America, your top brand for precision-engineered door hardware.
CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)