Grab Latches

Need Help Choosing?

Talk to an Expert

Explore Our Selection of Grab Latches

Sugatsune America has established a strong reputation for engineering precision-engineered latching solutions designed for consistent performance across architectural and industrial applications. That quality and precision extend to our selection of grab latches.

These expertly crafted products allow for the simple latching of drawers and cabinets with little effort and easy installation. The mechanisms we offer use spring force, rolling elements, or tension-based engagement to secure doors and panels without complex locking systems. Our versatile selection of grab latches comes in a variety of sizes and styles, allowing you to find the exact right latch for the job.

While mechanisms such as knuckle catches may appear simple, their performance relies on precise spring tension, material selection, and proper alignment.

The latches you purchase from Sugatsune are not only expertly made but also crafted from high-quality materials, ensuring your cabinets and drawers function properly for years to come. They are commonly specified for cabinetry, equipment enclosures, access panels, and commercial interiors requiring reliable, repeatable closure.

Contact Sugatsune’s Inside Sales team to consult on latch selection based on your application requirements and load conditions.

Variety of Latch Styles and Materials Built for Any Use

Grab latches are selected based on factors such as holding force, material compatibility, environmental exposure, and frequency of use. As you have come to expect from Sugatsune America's vast selection of hardware, we have an array of high-quality grab latches designed to solve your unique engineering challenge.

Depending on your specific requirements, you’re bound to find the best latch for your next project. For lightweight applications, plastic knuckle catches provide corrosion resistance and reduced weight while maintaining consistent holding force.

For higher load requirements or harsh environments, stainless steel latches provide increased strength, corrosion resistance, and long-term durability. In that case, we have a variety of stainless steel latches, including adjustable tension catches, that will fit the bill. 

Each latch type is engineered to meet specific performance requirements across a range of applications.

Proper latch selection ensures consistent engagement, minimizes wear, and maintains alignment under repeated use.

FAQs

When is it best to use a plastic door catch?

Many people might assume a plastic door catch will be too flimsy for their needs. While it is true that plastic isn’t as strong as stainless steel, Sugatsune’s plastic catches, including ball catches, are still incredibly durable and are a wonderful choice for many projects.

Because they use plastic, these latches are lightweight, cost-effective, and corrosion-resistant. They are great for use in many projects seeking to secure many commonly used drawers and doors.

You can often find plastic latches used the most in many applications, because they are lightweight, easy to install, and durable. They are also more economical than other materials, but if crafted well, you don’t sacrifice too much in durability.

What are some advantages of using grab latches versus other securing mechanisms?

Often, when people think of latches used for doors or drawers, they imagine complicated locking mechanisms.

Sure, these have their place in many projects. However, grab latches, including roller catches, have the advantage of simplicity. These grabber latches securely shut a door or drawer, ensuring it won’t open unless pulled, while eliminating the need for overly complex mechanisms.

They are simple to install, lightweight, easy to adjust, and incredibly durable. For drawers or doors that need to be opened and closed quickly and frequently, grabber latches are ideal.

Make sure to check that the hold force of the latch is right for your project.

What type of project would require a tension latch?

A tension latch, as the name suggests, is a latching mechanism that uses tension to create a secure closing.

Sugatsune offers a variety of tension latches, including an adjustable option, for projects that want the simplicity of a grab latch with the enhanced durability of stainless steel. These latches are also great for applications where the drawer or door might be subjected to movement and vibrations.

How do you select the correct grab latch for an application?

Selection depends on required holding force, material compatibility, environmental exposure, and frequency of use. Engineers should also consider alignment tolerances and whether vibration or movement will affect latch performance.

Ready To Take Your Project to the Next Level?