Sugatsune’s Latest Hinge Streamlines the Hidden Door
Posted On Oct 23rd 2025
Posted On Oct 23rd 2025
Posted On Oct 23rd 2025

The latest hinge from Sugatsune drastically reduces routing—ideal for retrofits and refined finishes.
By: Metropolis Staff
A concealed door is a study in restraint—a surface uninterrupted, hardware tucked out of sight, a threshold that slips from view. But concealing a door has long required time-consuming prep and exacting millwork. Sugatsune Concealed Hinges, known for their versatility and three-way adjustability, rewrite that process with the HES2S Surface Mount Concealed Hinge—an adjustable concealed hinge that mounts directly to the frame's surface, streamlining the path to a flush, refined finish.
The HES2S concealed hinge is the latest in Sugatsune’s evolving line of concealed hinges, and its defining move is a simple one: surface mounting. Traditionally, creating a hidden door meant carefully routing out both the frame and the door—a messy, time-intensive process often impractical for retrofits. This new hinge changes that. Routing only the door side, screws directly into the frame side, eliminating the need for cutting or routing and keeping installation clean and efficient.
“Like we did back in 1992 when we introduced adjustable concealed hinges for doors, the HES2S exemplifies how Sugatsune creates satisfaction and convenience for both professionals and do-it-yourselfers,” said Curtis Nakamura, Senior Vice President at Sugatsune America. “By eliminating the need to route out the frames, you can mortise these hinges into doors at the shop or in the garage, avoiding unnecessary cleanup inside the house.”

That efficiency maintains the performance level expected from Sugatsune. The HES2S concealed hinge is fully three-way adjustable—horizontally, vertically, and in depth—making it easier to achieve the clean reveal that defines a successful concealed door. Designed to work with 1-3/8-inch-thick doors and thicker, it opens up hidden-door possibilities for standard residential dimensions, allowing architects and builders to integrate minimalist detailing even in existing spaces.
This model supports up to 88 pounds with two hinges, and up to 110 pounds with three. For installers, that means it can carry a substantial solid-core door while remaining virtually invisible. It also pairs easily with shop-based preparation: the door can be mortised off-site, then quickly installed without touching the existing frame—an ideal condition for remodels, where minimizing disruption is essential. Sugatsune also supports the installation process with Denpo's Templates, available on Sugatsune’s website. Sugatsune Hinges are also found in the Shaper Tools’ hardware catalog—offering precision jigs and digital routing aids to ensure clean alignment, especially on larger projects.

Sugatsune has built its reputation on this kind of problem-solving. The company introduced adjustable concealed hinges in 1992, and this surface-mounted iteration expands that legacy by making the look of architectural minimalism look easier to achieve. Backed by Sugatsune’s legacy and drive for innovation, the HES2S Concealed Hinge removes a long-standing barrier to concealed hardware, translating that expertise into something simpler, cleaner, and more accessible for today’s interiors.
CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)