Casters

Backed by decades of research and development, Sugatsune offers caster and wheels designed to support highly specialized requirements. Be sure to check out our line-up of Powermax® wheels.

Need Help Choosing?

Talk to an Expert

Durable Design Solutions


Whether you’re looking for shock-absorbing casters or you are building specialized AGV equipment, you’ll find an impressive range of caster hardware to choose from. Twin-wheel swivel casters provide stability while making it easy to change direction. They’ve become a favorite for chairs, desks, workbenches, and other furniture. Heavy-duty casters, including our newest Powermax® wheels, are an excellent choice for specialty equipment that requires the highest level of durability and dynamic load capacity such as logistic equipment, automated guided vehicles, and conveyor systems.

High-Quality Engineering Since 1930


Since 1930, Sugatsune has been a trusted source for precision-engineered original hardware solutions worldwide. From architectural and furniture hardware to industrial components for industries including food, medical equipment, transportation, and aerospace, you can find the rightsolution to help build your creations. Sugatsune America is AS9120 B and ISO9001;2015 certified and distributes unique products to create convenience and satisfaction for people.

Learn more about our caster hardware and over 6,000 products by accessing our resources, extensive product literature, or contact our experts to find the right solution for your project applications.

FAQs

What are the key considerations when selecting the right casters for my application?

Casters affect several factors, such as performance and longevity. They’re also critical to safety. First, determine the total load you need to move. This includes the object itself and its contents. Divide that weight by the number of casters you plan to use. In most cases, that will be four. Then you should include a margin of safety; this is a buffer between the unit load and the caster capacity.

Next, you’ll need to think about the operational environment. Is the floor smooth? Will the caster need to roll over uneven surfaces or gaps? Will debris impact the caster’s operation? Is there a need to consider the amount of particle generation, anti-static or high resistance for tearing. The answers to these questions should influence the wheel material, type, and even diameter in many cases. For example, our low-profile heavy-duty casters handle heavy loads in tight spaces. Consider our dual brake casters for improved safety on slopes or for equipment that must remain stationary. Sugatsune America offers various types of casters, including those intended for high temperatures or corrosion resistance. Do consider usage frequency. A caster for a cart in constant use will have different specs from one for a rarely moved workbench, for example.

How do different caster materials and finishes affect their performance?

The material used for a caster’s wheel and frame impacts its performance. It also factors in durability and suitability for specific environments. For instance, a stainless steel roller caster would be a good choice for corrosive environments. It would work well in the food service and pharmaceutical industries. Do you need a high-capacity and floor-friendly option? What about the wear and durability requirements you have? High-quality polyurethane elastomer wheels are recommended to support heavy loads where wheel degradation is of concern. You might opt for rubber wheels for more conventional applications where heat isn’t as much of a concern.

The caster materials and finishes go beyond the wheel itself. Consider the frame or housing as well. These are often fashioned from zinc-plated, plastics or powder-coated steel. Some are even made of high grade stainless steel. These are great for rust resistance and standing up to wear and tear for specialized applications.

What are the specialized features and functions of casters, and how do they benefit my operation?

Casters' features and functions solve specific operational challenges. The simplest example is the brake. Our dual brake casters, for instance, prevent the wheel from rolling and also lock the swivel. This completely stops the casters for maximum safety and stability. Another example is the kingpin. This critical part influences how a caster handles shock loads and rotational forces. Some dirty or dusty environments may call for specifying casters with sealed bearings.

When selecting casters, think carefully about where and how you'll implement them. Do you have stringent requirements such as heavy loads or sanitary spaces? Go with a heavy-duty, stainless steel option. Do you need casters that can be separated for easier upkeep? Parts-separable casters are your solution. Knowing what’s required allows you to understand which specialized features are right for your application.

Ready To Take Your Project to the Next Level?