The World’s First Surface Mount Hidden Door Hinge Just Got Better!
Posted On Jun 23rd 2025
Posted On Jun 23rd 2025
Posted On Jun 23rd 2025
Media Contact:
Curtis Nakamura
Tel: 562.544.8909
Email: c.nakamura@sugatsune.com
Sugatsune’s Introduces the HES2S-150-A110 to It’s HES Line-Up.
For Immediate Release – Carson, CA Sugatsune, a global leader in precision-engineered hardware solutions, is proud to announce the launch of the HES2S-150-A110 surface mounted hidden door hinge designed to meet the needs of homeowners, contractors, and builders seeking a functional and easy-to-install solution. A follow up to its predecessor, the All New HES2S door hinge was created to accommodate 1-3/8” thick doors making it a great solution for upgrading residential doors without having to replace existing door frames.
“Like we did back in 1992 when we introduced adjustable concealed hinges for doors, the HES2S-150-A110 exemplifies how Sugatsune creates satisfaction and convenience for both professionals and do-it yourselfers,” said Curtis Nakamura, Senior Vice President at Sugatsune America. “By eliminating the need to route out the frames, you can mortise these hinges into doors at the shop or in the garage, avoiding unnecessary clean up inside the house.”
Key Features of the HES2S-150-A110:
With the growing trend of minimalistic designs and the rising popularity of hidden doors, the demand for hardware that can offer a clean, uninterrupted aesthetic has never been greater. Sugatsune created its surface mounted HES hinges to provide a faster, cleaner and more efficient way for installations. The HES2S-150-A110 now available for purchase through Sugatusne’s authorized distributors or visit us online at www.sugatsune.com.

About Sugatsune America, Inc.
With a heritage dating back to 1930 and established in 1982, Sugatsune America Inc. is AS9120 B; ISO 9001:2015 certified and has a rich tradition of manufacturing and distributing Japanese quality hardware. Sugatsune America stocks over 6,000 unique parts locally in the U.S. to provide the highest level of service. LAMP® is a registered trademark of Sugatsune Kogyo, Inc. For more information, visit www.sugatsune.com. Connect with Sugatsune America via Facebook (facebook.com/sugatsune), Instagram (instagram.com/sugatsuneamerica) and Twitter (twitter.com/sugatsune).
North American Headquarters:
18101 Savarona Way
Carson, CA 90746
Tel: 310.329.6373, 800.562.5267 (USA only)
Email: sales@sugatsune.com
CAD files are available on each product’s detail page. Click the “CAD/BIM Files” tab, located in the middle of the page to download the different formats. If CAD files are not available for a specific component, please contact our Support Team
Toll Free: (800) 562-5267 (U.S.A. only)